cancel
Showing results for 
Search instead for 
Did you mean: 

Sine wave generator using DAC - how to obtain exact results?

imalamoud
Associate
Posted on September 30, 2016 at 18:14

Hello,

I am trying to create sine wave generator using DAC and DMA based on STM32L476.

The goal is to obtain exactly 100KHZ, 10KHZ frequencies with maximum possible number of samples.

Thus I have set APB timer for DAC to 72MHZ, timer period to 15 and sample sizes to 48 for 100kHz and 480 for 10kHz.  This combination gives ideal frequency results.

However I need more than 480 samples for 10Khz.

If the sample pool is set to say 800, timer period to 9 then the result frequency is never exact there is en error of 1-2%. 

Why is that? Does the DAC/Timer combination require some special timing considerations?

1 REPLY 1
Posted on September 30, 2016 at 19:58

Period is normally an N-1 value, if you set it to 15 (0..15) it is dividing by 16. 72000000/16 = 4500000, 72000000/10 = 720000

Show your code, it is a lot easier than guessing.

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..