2016-09-19 03:41 PM
I am trying to change the sector security status of my RF sectors in I2C mode using the provided m24lr drivers, but it’s not working. Below is my code:
M24LR_SECTOR_SEC sss_write;
M24LR_SECTOR_SEC sss_read;
// unlock sector
sss_write.SectorLock = 0;
// use first password
sss_write.PassCtrl = 1;
// cannot write without password
sss_write.RW_Protection = 0;
NFCTAG_StatusTypeDef status = NDEF_OK;
uint32_t password = 0;
// present password
status = BSP_NFCTAG_GetExtended_Drv()->PresentI2CPassword(password);
wait_ms(1000);
for (int i = 0; i <
4
; i++)
{
status
=
BSP_NFCTAG_GetExtended_Drv
()->WriteSSSx((uint8_t)i, &sss_write);
BSP_NFCTAG_GetExtended_Drv()->ReadSSSx((uint8_t) i, &sss_read);
}
I first present the I2C password, which should be 0 because I haven’t changed it since receiving it. Afterward, I use the m24lr functions to write/read each sector’s SSS. However, even though the code runs and the status is always NDEF_OK, the sector security statuses never change. How can I fix this? I am using the Nucleo-NFC02A1 tag, which uses M24LR04E-R.
Solved! Go to Solution.
2016-09-20 05:12 AM
Hello on.brian,
There is a bug in thePresentI2CPassword
function (located in Drivers/BSP/Components/M24LR/m24lr.c)NFCTAG_StatusTypeDef M24LR_i2c_PresentI2CPassword( const uint32_t PassWord )
{ uint8_t ai2c_message[9] = {0}; uint8_t i; /* Build I2C Message with Password + Validation code 0x09 + Password */ ai2c_message[4] = 0x09; i = 0; while( i < 4 ) { ai2c_message[i] = ( PassWord >> (i * 😎 ) & 0xFF; ai2c_message[i + 5] = ( PassWord >> (i * 😎 ) & 0xFF; i++; }; /* Present password to M24LR */ return M24LR_i2c_WriteRegister( ai2c_message, M24LR_I2C_PWD_REG, 9 ); } the M24LR_i2c_WriteRegister function is used to write data to a register. To fix your problem you just have to replace the last line of this function with: return M24lr_IO_MemWrite( ai2c_message, M24LR_ADDR_SYST_I2C, M24LR_I2C_PWD_REG, 9 );
and the present password function should work. We will fix it in a next release. Second point, you need to initialize the driver pointer by using the init function before using any M24LR functions: (for example)/* Init M24LR driver */
while( BSP_NFCTAG_Init( ) != NFCTAG_OK ); I hope this will help you, kind regards.2016-09-20 05:12 AM
Hello on.brian,
There is a bug in thePresentI2CPassword
function (located in Drivers/BSP/Components/M24LR/m24lr.c)NFCTAG_StatusTypeDef M24LR_i2c_PresentI2CPassword( const uint32_t PassWord )
{ uint8_t ai2c_message[9] = {0}; uint8_t i; /* Build I2C Message with Password + Validation code 0x09 + Password */ ai2c_message[4] = 0x09; i = 0; while( i < 4 ) { ai2c_message[i] = ( PassWord >> (i * 😎 ) & 0xFF; ai2c_message[i + 5] = ( PassWord >> (i * 😎 ) & 0xFF; i++; }; /* Present password to M24LR */ return M24LR_i2c_WriteRegister( ai2c_message, M24LR_I2C_PWD_REG, 9 ); } the M24LR_i2c_WriteRegister function is used to write data to a register. To fix your problem you just have to replace the last line of this function with: return M24lr_IO_MemWrite( ai2c_message, M24LR_ADDR_SYST_I2C, M24LR_I2C_PWD_REG, 9 );
and the present password function should work. We will fix it in a next release. Second point, you need to initialize the driver pointer by using the init function before using any M24LR functions: (for example)/* Init M24LR driver */
while( BSP_NFCTAG_Init( ) != NFCTAG_OK ); I hope this will help you, kind regards.2016-09-20 10:26 AM
That fixed it! Thank you.