cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L476VGT6 STM32CubeMX 4.16.1 RAM linker script bug

sneal
Associate II
Posted on September 20, 2016 at 11:47

Have just updated to STM32CubeMX 4.16.1 and now the

STM32L476VGT6 linker script doesn't work.

linker script is set up for RAM1 and RAM2 in the memory area but not in the sections.

Had to rename RAM1 as RAM and manually enter RAM2 entries in order for the program to link.

Please fix

#!stm32-!cubemx-!bug
2 REPLIES 2
Nesrine M_O
Lead II
Posted on September 20, 2016 at 18:22

Hi neal.sue,

The issue has been reported internally.

-Syrine-

stm32cube-t
Senior III
Posted on October 07, 2016 at 18:48

Dear user,

This is fixed in next 4.17 release.