cancel
Showing results for 
Search instead for 
Did you mean: 

I think LDO Power is lack on STM32F746-DISCO Board.

JongOk Baek
Associate III
Posted on March 17, 2017 at 02:07

I test audio recorder/player on STM32F746-DISCO board.

So, WM8944(codec) drive speaker(2W) out.

But, TFT-LCD was break sometimes at full volume level.

So, I think LDO Power is lack on STM32F746-DISCO board.

1 REPLY 1
Nesrine M_O
Lead II
Posted on March 17, 2017 at 11:48

Hi

Baek.JongOk

,

  • Could you precise the STM32F7 cube version in which you have found the issue. So, we can verify it.
  • Otherwise,A touch screen interface is used to launch record process, to change input volume, pause record and to quit record menu by pressing Stop button: refer to application readme file for more details.

-Nesrine-