2017-03-16 06:14 PM
Hello.
I want to know more specification of STM32H7 series.
But, Information was not in ST site.
So I want to get datasheet and reference manual for STM32H7.
If it is possible to share, could you open more information.
I am waiting...
2017-03-17 03:30 AM
Hi
Baek.JongOk
,We are glad to see
your interest on the new STM3H7series.
As said during the announcement, the STM32H7 variants will become available along Q2-2
https://community.st.com/0D50X00009XkihHSAR
-Nesrine-
2017-03-17 05:00 AM
Glimpses of information get available, as STM contributes to the Linux kernel:
- [PATCH 0/5] Add STM32 DMAMUX support
-
https://lkml.org/lkml/2017/3/15/143
Why is general release of chip coupled to release of reference manual?
2017-03-17 05:20 AM
Why is general release of chip coupled to release of reference manual?
My guess - to keep the Errata documents short ... 😉
2017-04-25 11:31 AM
Is there any information about the release dates in lqfp208 package?)
2017-07-08 05:55 AM
Hey there,
Q2 is already gone! Are there any new informations about the release date for the h7?
Greetings!
2017-07-09 02:46 PM
Q2 is gone indeed. ST, please update the release info!
2017-07-09 11:38 PM
The Keremi newsletter (www<dot>keremi<dot>com) from last states:
STMicroelectronics removed the STM32H753 in the higher temperature grade from the site.
Seems there is still ongoing development and validation ...
2017-07-14 05:08 PM
Looked at errata, current revision is super buggy. I guess that is the answer why ST basically went silent about it.
In the next revision all of the bugs except one either marked as absent or has workaround. Hope they release it soon.
2017-07-16 09:57 AM
Dears,
You can check our web site and this new family is at evaluation phase and at production for OEM and few customers, so not yet in full production for all mass market customers. Full validation and qualification of new Technology Flash node of our STM32 MCUs is very important for us and for our customers {You 😉 } as we did in the past to all previous series : 180nm, then 130nm/110nm, then 90nm ( STM32F2/F4/F7 and STM32L4) and now 40nm with STM32H7xx.
Stay Tuned with us, you will release information on our web site, when we are ready !
Cheers,
STOne-32.