cancel
Showing results for 
Search instead for 
Did you mean: 

Getting Cosmic C setup with STVD

wfd
Associate II
Posted on September 28, 2016 at 15:36

I've downloaded STVD, installed it, Downloaded Cosmic C, installed it and downloaded en.stsw-stm8069.zip (standard peripheral library) Now. I cannot for the life of me get this thing working. I opened the .stw project within the unzipped std perph lib and when I build the stm8s105 project I get ''The Executable Cannot be found'' you can fix it by edit...... 

I try and fix it but I have no idea what it wants me to do.

Thanks 

Bill

#stm8s-discovery
1 REPLY 1
Ian Legg
Senior
Posted on September 29, 2016 at 11:26

Hi Bill,

When a project is added to the workspace it will ask which toolchain one is using. Alternatively you can set it in Project->Settings (General tab). Obviously the root path needs to be set to where ever you installed the toolchain.

Hope that helps.

Thanks,

Ian