2016-09-28 10:51 AM
Hello,
We are using a STC3115 in one of our designs. The problem is that it does not start up.
I read:
https://github.com/st-sw/STC3115GenericDriver/wiki/STC3115-FAQ
It looks like the problem is that the BATD is 'high'. I tried to force it low by connecting it to ground through a 1K resistor. However, the output of BATD is still 3.7V. Is there a way I can force it to become 'low'?
On the software side:
- I can communicate via I2C. The counter value reads: 1. So it seems that it starts, but then stops.
- A soft reset does not help
- I call BatterMonitorInit once
BatteryReadStateOfCharge is called every 500 ms.
- This results in the following o
utput:
My question is, why does it not start? Is
there something else i need to initialise?
Code
void BatteryMonitorInit(TI2CWriteReadFunction I2CWriteReadFunction)
{
I2CWriteRead = I2CWriteReadFunction;
TxBuffer[0] = 1; //regctrl
TxBuffer[1] = 0; //reset
I2CWriteRead(TxBuffer, 2, RxBuffer, 0);
// nrf_delay_ms(10);
//write REG_CC_CNF
TxBuffer[0] = REG_CC_CNF;
TxBuffer[1] = 210; //466
TxBuffer[2] = 1;
I2CWriteRead(TxBuffer, 3, RxBuffer, 0);
//write REG_VM_CNF
TxBuffer[0] = REG_VM_CNF;
TxBuffer[1] = 157; //157
TxBuffer[2] = 0;
I2CWriteRead(TxBuffer, 3, RxBuffer, 0);
TxBuffer[0] = REG_MODE;
TxBuffer[1] = 1+16;
I2CWriteRead(TxBuffer, 2, RxBuffer, 0);
}
uint8_t BatteryMonitorReadStateOfCharge(void)
{
TxBuffer[0] = REG_SOC;
I2CWriteRead(TxBuffer, 1, RxBuffer, 2);
uint16_t StateOfCharge = (RxBuffer[1] << 😎 + RxBuffer[0];
dbg(''rx[1]:%d\n'',RxBuffer[1]);
dbg(''rx[0]:%d\n'',RxBuffer[0]);
uint8_t StateOfChargePercentage = StateOfCharge >> 9;
TxBuffer[0] = 1; //regctrl
I2CWriteRead(TxBuffer, 1, RxBuffer, 1);
dbg(''REG_CTRL\n'')
dbg(''rx[0]:%d\n'',RxBuffer[0]);
TxBuffer[0] = 0; //regmode
I2CWriteRead(TxBuffer, 1, RxBuffer, 1);
dbg(''REG_MODE\n'')
dbg(''rx[0]:%d\n'',RxBuffer[0]);
TxBuffer[0] = 4;
I2CWriteRead(TxBuffer, 1, RxBuffer, 2);
dbg(''Counter\n'');
dbg(''rx[0]:%d\n'',RxBuffer[0]);
dbg(''rx[1]:%d\n'',RxBuffer[1]);
TxBuffer[0] = 8; //reg voltage
I2CWriteRead(TxBuffer, 1, RxBuffer, 2);
dbg(''batt voltage\n'');
dbg(''rx[1]:%d\n'',RxBuffer[1]);
dbg(''rx[0]:%d\n'',RxBuffer[0]);
TxBuffer[0] = 13; //reg open circuit voltage
I2CWriteRead(TxBuffer, 1, RxBuffer, 2);
dbg(''Open circuit voltage\n'');
dbg(''rx[1]:%d\n'',RxBuffer[1]);
dbg(''rx[0]:%d\n'',RxBuffer[0]);
TxBuffer[0] = 22; //reg relax
I2CWriteRead(TxBuffer, 1, RxBuffer, 1);
dbg(''relax counter\n'');
dbg(''rx[0]:%d\n'',RxBuffer[0]);
return StateOfChargePercentage;
}
Resulting Output:
SOC
rx[1]:58
rx[0]:168
REG_CTRL
rx[0]:4
REG_MODE
rx[0]:17
Counter
rx[0]:1
rx[1]:0
batt voltage
rx[1]:6
rx[0]:173
Open circuit voltage
rx[1]:26
rx[0]:180
relax counter
rx[0]:120
result 29
SOC
rx[1]:58
rx[0]:160
REG_CTRL
rx[0]:4
REG_MODE
rx[0]:17
Counter
rx[0]:2
rx[1]:0
batt voltage
rx[1]:6
rx[0]:162
Open circuit voltage
rx[1]:26
rx[0]:179
relax counter
rx[0]:120
#stc3115-issue-startup2016-09-29 09:17 AM
Hi
I'm struggling with a problem that might be related. In my HW the BATD pin is pulled high. That's incorrect, I know. But the symptoms are that there are problems with I2C write operations. Registers are read correctly, e.g. the device ID, but when running the driver downloaded from the manufacturer's site, register writes to REG_ALARM_VOLTAGE and REG_RAM0 fail. STM32F4 HAL reports HAL_I2C_ERROR_AF, which apparently means that STC3115 does not ack the write.Are you able to write into those registers?2017-12-07 04:59 PM
Hello,
As long a the BATD pin is not pulled-down, the STC3115 will not start the battery monitoring because it detects that no battery is connected.You can read the 'BATFAIL' bit in register REG_CTRL (@ADDRESS 1) to verify that the issue is due to battery detection.
If BATFAIL == 1, it means the STC3115 has detected an error.Best regards.
2017-12-07 06:09 PM
Hi,
If you can read STC3115 registers, it means the I2C write sequence should work, because an I2C random Read sequence always start with a Write.
So it seems the issue is coming from your Write implementation on the STM32 side.
The STC3115 Slave address is 8-bit (7-bit address, with a R/W bit at the end). It is not a 10-bit address like some EEPROM memories. So check the STM32 I2C master interface is not configured for 10-bit devices.
Also, when you perform a I2C Write, check that the R/W bit is set to 0.