2016-10-09 12:54 PM
Hi everyone, i have problem with a something project, i dont have comunication with microsd card on my board, my debug stay on function wait ready and next rcvr_spi(), and nothing to do ;/ i dont know where is problem,
i paste my configuration. my connect : CS - PE15, SCK - PB13, MISO PB14, MOSI PB15, i use coocox for comiple and debugMAIN[code]int main( void ){ SystemInit(); SPI_SD_Init(); fresult = f_mount( 0, &fatfs); fresult = f_open( &plik, ''demo.wav'', FA_OPEN_EXISTING | FA_READ ); if( fresult == FR_OK ) { //fresult = f_read(&plik, void * buffor, 17, &zapisanych_bajtow); fresult = f_read( &plik, ( void * ) buffor2, 112940, &odczytanych_bajtow ); } fresult = f_close( &plik );}[/code]SPI_SD[code]void SPI_SD_Init( void ) //inicialize spi{ GPIO_InitTypeDef GPIO_InitStructure; SPI_InitTypeDef SPI_InitStructure; volatile BYTE dummyread; // Konfiguracja wyprowadzen i kontrolera SPI:config output spi /* Enable GPIO clock for CS */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE, ENABLE); /* Enable SPI clock, SPI2 */ // Wlaczenie sygnalow zegarowych dla peryferiowclock for peripherials RCC_APB1PeriphClockCmd( RCC_APB1Periph_SPI2, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE ); GPIO_PinAFConfig(GPIOB, GPIO_PinSource13, GPIO_AF_SPI2 ); GPIO_PinAFConfig(GPIOB, GPIO_PinSource14, GPIO_AF_SPI2); GPIO_PinAFConfig(GPIOB, GPIO_PinSource15, GPIO_AF_SPI2 ); // PE15 CS GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOE, &GPIO_InitStructure); DESELECT_SD(); //SCK, MISO and MOSI SD GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOB, &GPIO_InitStructure); // Konfiguracja SPI enable spi SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_High; // low ? SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_4; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_Init(SPI2, &SPI_InitStructure); // Wlacz SPI SPI_Cmd(SPI2, ENABLE); while (SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_TXE) == RESET) { ; } dummyread = SPI_ReceiveData(SPI2);}[/code]ODEBRANIE BAJTU I WYSLANIE[code]staticvoid xmit_spi (uint8_t outB) // Wyslanie bajtu do SPI{ u8 Data = 0; while (SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_TXE) == RESET); SPI_I2S_SendData(SPI2, Data);}staticBYTE rcvr_spi (void) // Odebranie bajtu z SPI{ u8 Data = 0; // Wysłanie 0xFF while (SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_TXE) == RESET); SPI_I2S_SendData(SPI2, 0xFF); // odebranie bajtu while (SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_RXNE) == RESET); Data = SPI_I2S_ReceiveData(SPI2); return Data;}staticBYTE wait_ready (void){ BYTE res; Timer2 = 50; /* Wait for ready in timeout of 500ms */ rcvr_spi(); do res = rcvr_spi(); while ((res != 0xFF) && Timer2); return res;}[/code][code]staticvoid power_on (void){ u8 i, cmd_arg[6]; u32 Count = 0xFFF; // Inicjalizacja karty i przelaczenie w tryb SPI: DESELECT_SD(); // CS = 1 for (i = 0; i < 10; i++) xmit_spi(0xFF); // Wyslij 0xFF 10 razy = 80 cykli zegarowych // (wymaganych co najmniej 74 cykli) SELECT_SD(); // CS = 0 // Przygotowanie ramki inicjujacej do wyslania cmd_arg[0] = (CMD0 | 0x40); cmd_arg[1] = 0; // Argument komendy cmd_arg[2] = 0; // nawet, gdy komenda go nie ma cmd_arg[3] = 0; // musi zostac wyslany w postaci zer cmd_arg[4] = 0; cmd_arg[5] = 0x95; // CRC = 0x95 for (i = 0; i < 6; i++) // Wyslanie ramki xmit_spi(cmd_arg[i]); while ((rcvr_spi() != 0x01) && Count) // Czeka na 0x01 Count--; DESELECT_SD(); // CS = 1 xmit_spi( 0XFF ); // Wyslij 0xFF PowerFlag = 1;}[/code][/code]2016-10-09 04:05 PM
You configure PE12 not PE15
There doesn't appear to be any timeout counter/interrupt implemented, so it won't leave the loop. You might want to instrument the code to see what comes back, and review that in the context of the MMC/SD Card protocol documentation.2016-10-18 09:30 AM
2016-10-18 12:04 PM
can you help me ?
I've provided SDIO examples for the STM32F4-DISCO board, unfortunately I can't expend my resources on debugging your code. If the bits are always zero one might double check the peripheral clocks, but don't look at the SPI2 peripheral through a Peripheral View in the debugger, it will break/clear bits. The debugger can be very invasive at a peripheral level.
2016-10-23 10:45 AM
At this moment i dont know..i do this everythin... i have on board only pull up resisotr on CS PIN 10K to 3.3 V.
When i call function fresult = f_mount i back FR_OK but when i call fresult = f_open i have problem on function rcvr_spi() and next still stay on function wait_ready and line '' while ((res != 0xFF) && Timer2); ''when i call function before f_mount and f_open i havefresult = disk_initialize() -> FR_DISK_ERRfresult = disk_read() -> FR_NO_FILEand when i call only function disk_initialize(0) he still stay always ''while ((res != 0xFF) && Timer2);''2016-10-23 12:41 PM