cancel
Showing results for 
Search instead for 
Did you mean: 

bug report for X-CUBE-SPN7

bluenow1896
Associate III
Posted on June 13, 2018 at 20:20

Hi ST support and developer,

  I have a small bug report for X-CUBE-SPN7, in the project of examples, 

  Projects/Multi/Examples/MotorControl/SW4STM32/STM32F302R8-Nucleo,  the include path has set to

../../../../../../Drivers/BSP/Components/L6230  , instead of ../../../../../../Drivers/BSP/Components/l6230 :

  This causes build failed on Linux.

  On Windows it is OK as Windows could treat 'L' and 'l' to be same in the path and file name, but Linux will see them different.

-Andy

0 REPLIES 0