cancel
Showing results for 
Search instead for 
Did you mean: 

Removing the spwf01sx cgi files.

pouya
Associate II
Posted on December 08, 2016 at 09:13

Hi, 

I was wondering that if it is possible to delete the HTML and CGI file system from the module.?

P.S: I can see from the documentation that it is possible to disable/enable the feature. My concern is to permanently delete the files.

#cgi
1 REPLY 1
Posted on December 10, 2016 at 15:17

Hi,

cannot delete files inside STM32 flash (so, HTML and/or CGI). The ones marked as 'I' from AT+S.FSL command.

You can delete HTML inside external flash, if using SPWF01Sx.11, by AT+S.HTTPDFSERASE. The ones marked as 'E' from AT+S.FSL command.

Regards

jerry