cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 VCP plug and play

danielspronk9
Associate II
Posted on April 07, 2017 at 08:05

Hello,

im using the STM32F407 DIS with CubeMX to generate a USB CDC device.

All works fine but if i unplug the STM32f407 and then plug in, Windows 10 didnt detect the driver(just unknown USB-Device)

i have to reset the STM and then Windows detect the driver.

What can i do to use the STM32 with plug and play?

i use VCP 1.4

#vcp-stm32f4 #cubemx-f4
1 REPLY 1
T J
Lead
Posted on April 08, 2017 at 02:30

whats wrong with plug and pray ?  thanks to Bill, we have got use to Re-Booting...

if you look below on this page, it has related content.

you can search the previously answered questions, there is a goldmine of information here.