cancel
Showing results for 
Search instead for 
Did you mean: 

stm32 timer captur

mahdi zamani
Associate II
Posted on November 20, 2016 at 07:58

hey all

i configed timer 3 whit this ....

formeasurement frecuncy in PA.7

void TIM3_Configuration(void){

RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);

TIM_ICInitTypeDef TIM_ICInitStructure;

TIM_ICInitStructure.TIM_Channel = TIM_Channel_2;

TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising;

TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI;

TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1;

TIM_ICInitStructure.TIM_ICFilter = 0x0;

TIM_ICInit(TIM3, &TIM_ICInitStructure);

/* TIM enable counter */

TIM_Cmd(TIM3, ENABLE);

/* Enable the CC2 Interrupt Request */

TIM_ITConfig(TIM3, TIM_IT_CC2, ENABLE);

NVIC_InitTypeDef NVIC_InitStructure;

/* Enable the TIM3 global Interrupt */

NVIC_InitStructure.NVIC_IRQChannel = TIM3_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

}

i read captur whit this code :

frq=TIM_GetCapture2(TIM3); but not work :(((

please help to me ...

thanks

2 REPLIES 2
Posted on November 20, 2016 at 08:37

Ok, so what are you seeing when you read the capture register, and what were you expecting to see?

Tends to be a time stamp of the time base, which advances, so you'd need to delta it.

Which STM32, they make a few versions these days.

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..
mahdi zamani
Associate II
Posted on November 20, 2016 at 08:55

void TIM3_Configuration(void){

RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);

TIM_ICInitTypeDef TIM_ICInitStructure;

TIM_ICInitStructure.TIM_Channel = TIM_Channel_2;

TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising;

TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI;

TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1;

TIM_ICInitStructure.TIM_ICFilter = 0x0;

TIM_ICInit(TIM3, &TIM_ICInitStructure);

/* TIM enable counter */

TIM_Cmd(TIM3, ENABLE);

/* Enable the CC2 Interrupt Request */

TIM_ITConfig(TIM3, TIM_IT_CC2, ENABLE);

NVIC_InitTypeDef NVIC_InitStructure;

/* Enable the TIM3 global Interrupt */

NVIC_InitStructure.NVIC_IRQChannel = TIM3_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

}

void assert_failed(uint8_t* file, uint32_t line)

{

/* User can add his own implementation to report the file name and line number,

ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */

while (1)

{}

}    complete programme can edite my program tomeasurement frequncy at PA.6 and write it to ''FRQQ''?  i downloaded sample for this but i cant work on it :( sorry itsthe first my project whit stm32 ... thanks