cancel
Showing results for 
Search instead for 
Did you mean: 

TRANSLATING ASSEMBLY CODE FROM HC05 TO ST7

gianfranco2
Associate II
Posted on March 07, 2003 at 04:52

TRANSLATING ASSEMBLY CODE FROM HC05 TO ST7

2 REPLIES 2
gianfranco2
Associate II
Posted on March 06, 2003 at 04:25

Dear Sir,

According to AN1106, it is possible translate the assembly code from Hc05 to ST7 using the ST free utility migr2st7.

I would like to know if it is also possible to use the same software in order to traslate from HC08 to ST7.

In fact, HC08 is compatible with HC05 core.

Thanks in advance for your copperation

Gianfranco

[ Questo Messaggio è stato Modificato da: dimarcog il 06-03-2003 08:56 ]

________________

Attachments :

1011096740.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I07E&d=%2Fa%2F0X0000000bTh%2F9jVnBEraWRPQGQRTxDQhNtgvdOonc5TA3Vxdh6mRb7k&asPdf=false
stephanie
Associate II
Posted on March 07, 2003 at 04:52

It should work. The best way is to try, but you can also have a quick look on the 2500adcb.h file (installed by the setup) to read all the treated directives.

Good migration!