cancel
Showing results for 
Search instead for 
Did you mean: 

STR71x Flash lib

sjo
Associate II
Posted on September 12, 2005 at 11:26

STR71x Flash lib

1 REPLY 1
sjo
Associate II
Posted on September 12, 2005 at 10:03

I have noticed a few more errors when using the Flash lib functions (v3.0).

FLASH_WritePrConfig - you are still using the TmpProtection variable which is not initialised.

you declare the function as FLASH_DebugPrConfig in the header, the function is defined as FLASH_PermanantDebugPrConfig in the source file.

Also when you release the next version of the library can you put the links back into the pdf as per previous releases, it was much easier to find a function in the older pdf docs (v1.2/v1.3).

Also when is the updated/corrected usb lib going to be released ?

Regards

sjo