cancel
Showing results for 
Search instead for 
Did you mean: 

ICC Debug Modul

janvi
Associate II
Posted on January 10, 2003 at 07:21

ICC Debug Modul

2 REPLIES 2
janvi
Associate II
Posted on January 05, 2003 at 14:06

I am somewhat confused choosing a ST7 what contains a DM Peripheral feature. The ICC Manual (V1.2) describes @page 16 that ''advanced'' ICC commands are requierd for ICDebug and medium and basic are for flash programming only.

How is it possible, that Table 1 page6 of same document describes the F561 with basic ICC but contains 1 DM?

Further I searched some datasheets including the F264 and some 2xx Manuals for the description of the breakpoint register address (DMBKx). Cannot find this in register map nor in peripheral descriptions.

Are there any CANflash with DM (64 pin Case) available? The F561 coming soon? (with DM?)

simms
Associate II
Posted on January 10, 2003 at 07:21

There's no DM on the F561, the ICC manual should be amended on this point. Other CAN ST7s don't have the DM function either.

HTH