cancel
Showing results for 
Search instead for 
Did you mean: 

ST92F150-EMU2 limitations

econfalonieri
Associate II
Posted on October 14, 2003 at 18:35

ST92F150-EMU2 limitations

2 REPLIES 2
econfalonieri
Associate II
Posted on May 17, 2011 at 11:35

Dear Sirs, I noticed on ST92F150 Datasheet (June 2003 - Rev. 1.4) that the emulator ST92F150-EMU2 supports also ST92F250 with some limitations reported in Table 71, Note1:

''The I²C 1 and the general purpose I/Os P3.0, P6.6 and P6.7 cannot be emulated by this emulator. Since the upper 128Kbytes of Flash memory are emulated with a RAM memory, the programming operations on the F4 and F5 Flash sectors are not emulated.''

I'm asking you if a future emulator version without these limitations has been planned. This is important for some of our customers.

Thanks in Advance

Best Regards.

Enrico
loic2
Associate II
Posted on May 17, 2011 at 11:35

You have more details on differences between ST92F250 and emulator in the AN1578 (Developing ST92F250 applications using the ST92F150-EMU2 Emulator).