cancel
Showing results for 
Search instead for 
Did you mean: 

ST7Flite - 7 segment displays

andys
Associate II
Posted on September 30, 2003 at 08:25

ST7Flite - 7 segment displays

2 REPLIES 2
andys
Associate II
Posted on September 29, 2003 at 13:04

Are thera any application notes about driving 7 segment displays?

Im using 2 shift registers (4094) and 4 x 7 segment displays.
simonharrison9
Associate II
Posted on September 30, 2003 at 08:25

Hi,

It's a little old now, but look at the

http://eu.st.com/stonline/books/pdf/docs/6623.pdf

At the back ( around page 280 ), is a project using 4094's driving LCD's.

I think the code to drive the 4094s is explained and/or included.

You should be able to port this to the FLITE very easily.

regards

Simon