cancel
Showing results for 
Search instead for 
Did you mean: 

Strap options for CPU Clock Multiplication (486 mode) - Atlas

mdesjardine
Associate II
Posted on September 18, 2003 at 13:33

Strap options for CPU Clock Multiplication (486 mode) - Atlas

3 REPLIES 3
mdesjardine
Associate II
Posted on September 10, 2003 at 20:19

Hi,

What happens if you have MD[14] = 0 and MD[40] = 1 on an Atlas? The datasheet indicates that this is a reserved setting. Any idea of what this reserved setting does and what speed the system will run at? Can it be used with HCLK = 66 MHz?
davidbellegarde9
Associate II
Posted on September 17, 2003 at 06:53

Hello,

The settings that you describe is for x3 mode but it cannot be used with HCLK=66MHz.
stephen239955_st
Associate II
Posted on September 18, 2003 at 13:33

Please be advized that the STPC Atlas does not support these multiplication factors and if they are selected will not be work reliably.