cancel
Showing results for 
Search instead for 
Did you mean: 

ST9+ Visual Debug v6.1.8 windows DLL error user32.dll relocated

scott239955
Associate II
Posted on April 10, 2007 at 15:24

ST9+ Visual Debug v6.1.8 windows DLL error user32.dll relocated

2 REPLIES 2
scott239955
Associate II
Posted on May 17, 2011 at 11:31

I have been using ST9+ Visual Debug v6.1.8 on WinXP for years now, but now I get a windows error stating that DLL error user32.dll was relocated in memory and application will not run. It states that C:\WINDOWS\System32\HHCTRL.OCX occupies the address and it is reserved for windows. This may have happened after a windows update.

I tried reinstalling the tool chain, but I still get the same error. Please help--I can not wipe the hard drive clean and start over.

I tried the newer version of the tool chain before when it was released, but I could not get it to run the code correctly. :-[

scott239955
Associate II
Posted on May 17, 2011 at 11:31

This is a Windows problem. A fix can be downloading from Microsoft that fixes the problem. The link is bellow:

http://support.microsoft.com/kb/935448/en-us

:D