cancel
Showing results for 
Search instead for 
Did you mean: 

ST72264G datasheet

mailtoarup
Associate II
Posted on February 11, 2004 at 04:55

ST72264G datasheet

2 REPLIES 2
mailtoarup
Associate II
Posted on February 11, 2004 at 01:48

dear sir,

I have some doubt regarding ''ST72264G'' datasheet.I have found some ambiguity in the ''Memory Map''(page 10) section.In that doc Memory map is divided into 5 parts-

* HW Registers(0000h-007fh)

* RAM(0080-017fh)

* Reserved(0180h-Dfffh)

* Program Memory(E000h-Ffdfh)

* Interrupt & Reset Vectors(FFE0h-FFFFh)

In the same page u have showed program memory is divided into 2 parts:

sector 1(E000h-EFFFh)

sector 0(F000h-FFFFh) which is reserved for interrupt & reset vectors.

while Program Memory space itself is E000h-FFDFh,then how can be one of its part sector 0 which is in the space F000h-FFFFh is lying outside the program memory space.

While already you have showed Progarm Memory and Reset & Interrupt vector space as two distinct part in the memory map,then why did u combine it with sector 0 of progarm memory.

Pls exaplain.And rectify it in your ST72264G Doc.

Regards,

Arup
jatin
Associate II
Posted on February 11, 2004 at 04:55

It does not impact the application anyway and it is same terminology which is used in all ST7 devices.