cancel
Showing results for 
Search instead for 
Did you mean: 

Programming Failed at address F5DF

tech4
Associate II
Posted on June 09, 2003 at 10:50

Programming Failed at address F5DF

4 REPLIES 4
tech4
Associate II
Posted on June 02, 2003 at 13:54

Hye,

I'm trying to program in ISP mode an ST72C215G2 via an ST7MDT1-DVP2 KIT. My OS is Windows XP Home edition... And just before achieving the programmation, it stopped on the error listed above.

Why ?! I tried on another PC under Windows 98...It works well !!!

Please, what can I do ?
shreya
Associate II
Posted on June 05, 2003 at 12:20

Hello,

What version of STVD7 are you using? I would suggest STVD7 2.5.2. During the installation process, you must have been asked for installation of parallel port driver. Is this driver installed?
tech4
Associate II
Posted on June 05, 2003 at 13:59

Hello,

I'm using the STVD7 V2.5.2, but the problem is with the STVP

Version 1.8. The parallel port driver is installed ?!
shreya
Associate II
Posted on June 09, 2003 at 10:50

Some suggestions :

1) The parallel port driver for the STVP7 should have been installed during STVP7. Please re-install and check.

2) Is the hardware of your kit updated?(Refer AN1363)