cancel
Showing results for 
Search instead for 
Did you mean: 

Unstable ADC reading result

irawan1
Associate II
Posted on January 17, 2006 at 03:16

Unstable ADC reading result

1 REPLY 1
irawan1
Associate II
Posted on May 17, 2011 at 12:09

Dear all,

i am using upsd3333d-80 pins, to measure voltage using adc ch0.

The voltage measured came from a voltage divider using resister 2M7 and 300K, and the range of the the voltage being measured is 0-2.5V at ADC input pin. The VRef is connected to TS431 that gives 3.04V. My problem is i always got varying result of ADC reading (2-3 bit error). Any hints or suggestion, will be appreciated.

thanks.