cancel
Showing results for 
Search instead for 
Did you mean: 

Which ST10 type can be insted of C167CS-LM from Infineon?

pichet
Associate II
Posted on May 19, 2003 at 22:27

Which ST10 type can be insted of C167CS-LM from Infineon?

2 REPLIES 2
pichet
Associate II
Posted on May 19, 2003 at 05:39

Hello

My customer have designed the automotive project that used C167CS-LM would like to changed to ST10 but didnot know which part no will compatible pin by pin and also want to know the old software used Keil C-Complier still used for ST10 or not?

BR's

JOM
maxime2399
Associate II
Posted on May 19, 2003 at 22:27

There nothing exactly equivalent but is two parts that could be used.

If you need 2 CAN, the ST10F269 will do the job. It has on top of that some built in Flash and a MAC cell. (see enclosed application note)

If you want a ROMless device the ST10R167 has one CAN bus only and could do the job.

Keil compiler fully support both devices.

________________

Attachments :

an1314__compare_C167_F269_.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0KI&d=%2Fa%2F0X0000000bXO%2F6f15WzwJPl14GgLq1KY5GvB2dobJYd82C1o0ieJgGHo&asPdf=false