cancel
Showing results for 
Search instead for 
Did you mean: 

ST7MDT10_EMU3 problem???

huaer2000
Associate II
Posted on September 28, 2004 at 10:38

ST7MDT10_EMU3 problem???

2 REPLIES 2
huaer2000
Associate II
Posted on September 28, 2004 at 04:58

Dear sir,

while I use St7MDT10-EMU3, there is an error messag like this.

** Connection error (usb://usb): gdi-error in hds:[10004]

no Communication with emulated mcu

Could anyone tell me how to solve this problem.

Best Regards,

Mucinterest
juhee
Associate II
Posted on September 28, 2004 at 10:38

There seems to be a connection error, so you can verify the following:

1. If you are using STVD7 3.0, In the Debug Instument Tab, select the Port at which you have connected the emulator. If you are using old version of STVD7, in the emulator settings select the Port correctly.

2. Try changing the Microconnect (If you have an Extra?)

3. Check the Flex-Cable that you are using