2008-02-18 11:06 PM
2011-05-17 12:49 AM
Hi all,
I start a design on STR912FAW44 and I'm using CAPS software to assign pins. But I've a problem to declare I2C0 as master. I2C0 on P2.0 and P2.1. I check registers values generated in conf.h file : :o #define GPIOIN2 0x1 #define GPIOOUT2 0x8 #define GPIO_DIR2 0x0 I don't understand why P2.0 is set as I2C0_CLKIN and P2.1 as I2C0_DOUT ? And why GPIOIN register set only P2.1 as output :-[ How can I declare I2C0 master mode with the 2 pins as ouput (2C0_CLKOUT and I2C0_DOUT) in CAPS ? Thanks in advance [ This message was edited by: jim06 on 07-02-2008 15:15 ]2011-05-17 12:49 AM
Hello Jim06,
I noticed the same problem using the I2C0 peripheral. With constants generated by the CAPS, I2C faild to work. So I modified the constants myself in the software (see below) resulting in a good working I2C device. GPIO2->DDR = GPIO_DIR2; SCU->GPIOOUT[2] = GPIOOUT2 | 0x2; // CAPS puts I2C SDA in input mode -> select alternate function SCU->GPIOTYPE[2] = GPIOTYPE2; SCU->GPIOIN[2] = GPIOIN2 | 0x2; // CAPS doesn't connect I2C SDA to the input: select alternative input 1 With following constants: #define GPIO_DIR2 0xC #define GPIOTYPE2 0x3 #define GPIOOUT2 0x58 #define GPIOIN2 0x1 Best regards, LouisKatorz2011-05-17 12:49 AM
Hi LouisKatorz,
Yes, I did the same fix to make works the I2C0. 😉 CAPS is very useful to start a design. It works properly for others functions, but it has to be modified to set I2C. Thanks. BR