cancel
Showing results for 
Search instead for 
Did you mean: 

stkit st622x win2000 problem

wojciech2
Associate II
Posted on August 20, 2003 at 06:57

stkit st622x win2000 problem

3 REPLIES 3
wojciech2
Associate II
Posted on August 11, 2003 at 05:36

Bad work on the win2000, cannot communicate with the device. With win98 is OK. Software ''Windows Epromer'' version 4.02 or 3.3, both is not working.

Can anybody help me?
jacques2
Associate II
Posted on August 11, 2003 at 10:20

See text below from the ST6 Windows Epromer 4.0.2 Release Note.

Make sure the NT parallel port driver is installed. This driver installs itself if not detected at the end of the windows epromer install. You should propably reinstall your windows eprommer software.

--------------------------------------------------------------

ST6 Windows Epromer can be installed on PCs and compatibles running with Windows ® 95,

Windows ® 98, Windows ® 2000 or Windows ® NT ® 4.0 operating systems.

Note: Installing WINDOWS EPROMER on a Windows ® NT or Windows ® 2000 machine for hardware

programming tools which use the parallel port on your host PC, will trigger the installation of the NT

Driver “STM Parallel Driver� if it has not yet been installed. In this case, administrator rights are

required.
wojciech2
Associate II
Posted on August 20, 2003 at 06:57

I installed this driver and reinstalled eprommer software. Is still not working.