cancel
Showing results for 
Search instead for 
Did you mean: 

ICP OPT Enable, ICP OPT Disable details usage.

alanlai1
Associate II
Posted on November 17, 2004 at 06:10

ICP OPT Enable, ICP OPT Disable details usage.

2 REPLIES 2
alanlai1
Associate II
Posted on November 12, 2004 at 13:37

Dear all,

ICP OPT Enable, ICP OPT Disable.

Recently, I knew that the ''ICP OPT Disable'' is useful when I need to disable the read out protection, but is it any more usage for this ''ICP OTP Disable''?

Thank you very much ~

jatin
Associate II
Posted on November 17, 2004 at 06:10

ICP Option byte enable/disable is used to select the clock source during ICP. With ICP option byte disable the clock is supplied by the source and with ICP option byte enable, the clock source programmed in the option bytes of the target micro will be taken into account.