cancel
Showing results for 
Search instead for 
Did you mean: 

STR7 complete datasheets

igorl
Associate II
Posted on July 31, 2004 at 02:25

STR7 complete datasheets

5 REPLIES 5
igorl
Associate II
Posted on June 11, 2004 at 06:30

Dear Moderator!

Can you, please, tell me where I can get complete datasheets if STR7 series microprocessors? The ones presented at ST's website are too poor to start developing.

Thank you in advance
subscriptions2
Associate II
Posted on June 16, 2004 at 17:20

Quote:

On 2004-06-11 10:09, RISC wrote:

Dera Igoron

The complete description of the STR71x series is guived in the

http://www.stmcu.com/mcdfiles/1082043493.pdf

Which at the very least is missing any description of the serial boot load process.

sjo
Associate II
Posted on June 17, 2004 at 06:44

The document required is ''STR71x Flash Programmer� mentioned on page 38.

It has as yet not been released by ST.

Regards

sjo
subscriptions2
Associate II
Posted on July 31, 2004 at 01:34

Quote:

On 2004-06-16 20:50, radsett wrote:

Quote:

On 2004-06-11 10:09, RISC wrote:

Dera Igoron

The complete description of the STR71x series is guived in the

http://www.stmcu.com/mcdfiles/1082043493.pdf

Which at the very least is missing any description of the serial boot load process.

And the latest revision appears to have even less information.

shinnlin
Associate II
Posted on July 31, 2004 at 02:25

The SystemMemory Boot Mode section is marked reserved in latest reference manual rev.3.

Therefore, section 2.2.2.1 in rev.2.1 is no longer exist.

What's going on ?