cancel
Showing results for 
Search instead for 
Did you mean: 

with and without marking A of uPSD3454EB40T6 ? USB affected!

hg-chen
Associate II
Posted on August 21, 2008 at 09:16

with and without marking A of uPSD3454EB40T6 ? USB affected!

1 REPLY 1
hg-chen
Associate II
Posted on May 17, 2011 at 11:52

according to the PCN attached, the marking A only related to bond pad re-layout,which should not affect the functionality,

1, however, the USB does perform OK with marking A, but failed in

PC cold boot without marking A! Is the USB function really the same

between these 2 chips!

2, the marking A should be newer since it is new revision, but the attached photos show the one without marking A is newer! Why?