cancel
Showing results for 
Search instead for 
Did you mean: 

no embedded loader inside STR9 and STR7 , right?

hg-chen
Associate II
Posted on July 16, 2008 at 14:24

no embedded loader inside STR9 and STR7 , right?

2 REPLIES 2
hg-chen
Associate II
Posted on May 17, 2011 at 09:54

just to make sure that there is not no embedded loader like STM32 inside STR9 and STR7 , right?

jpeacock2
Associate II
Posted on May 17, 2011 at 09:54

The STR750 has the ICP boot loader, which can load from a serial port. I never used it, but it's an option on the boot pins.