cancel
Showing results for 
Search instead for 
Did you mean: 

driving capability (Fan Out ) of the RESETOUT\ Pin ST10F269Z2Qx

ludger
Associate
Posted on November 19, 2003 at 11:34

driving capability (Fan Out ) of the RESETOUT\ Pin ST10F269Z2Qx

2 REPLIES 2
ludger
Associate
Posted on November 14, 2003 at 06:28

Hi everybody,

can someone please give me some information about the maximum current, which can be provided by the RESETOUT\ pin of a ST10F269Z2Qx?

I use the RESETOUT\ pin as an ENABLE signal connected to four AND gates an alredy destroyed three CPUs.

charles239955_st
Associate II
Posted on November 19, 2003 at 11:34

In the specification the output voltage levels Vol and Voh are defined at the respective values 0.45V and 2.4V when the current is 2.4mA. Refer to datasheet DC characteristics section pages 139-140.