cancel
Showing results for 
Search instead for 
Did you mean: 

RTC in dk3200 problem help!!!!!!!!!!

thewind60
Associate II
Posted on April 17, 2005 at 22:22

RTC in dk3200 problem help!!!!!!!!!!

3 REPLIES 3
thewind60
Associate II
Posted on May 17, 2011 at 11:57

help!!!!!!!!!!!!!!!!!!!!!!

i use the RTC example and i want that when i turn of the system the clock will keep updating , but it's not!!!! it's only remember the last time and show it then keep updating

why is that ???

real time clock nned to keep updating even the system is off no??

please help me

joseph2399
Associate II
Posted on May 17, 2011 at 11:57

Did you check the voltage level of the SNAPHAT battery on top of the ST-85 RTC chip?

jmullaney
Associate II
Posted on May 17, 2011 at 11:57

I am experiencing the exact same problem. Did you resolve the problem??? My SNAPHAT voltage is OK (~3.0V)