cancel
Showing results for 
Search instead for 
Did you mean: 

Application AN1763 ( batery supllier)

ricardof
Associate II
Posted on July 19, 2005 at 11:51

Application AN1763 ( batery supllier)

1 REPLY 1
ricardof
Associate II
Posted on May 17, 2011 at 12:07

I have a problem in my design with one uPSD3312, and sometimes the XDATA value changes, maybe the battery supplier is less than 2 volts that the manufacture ask for keep the dates ( I don´t think so ). Someone can tell me why in the application note 1763 in the schemaquic appear one coil of 100 uH and one capacitor of 104p. If I put this in my design I will eliminate problems with eventual noise in the battery supplier or not. Thanks.