cancel
Showing results for 
Search instead for 
Did you mean: 

psdExpress upsd3300

hpaskal
Associate II
Posted on April 01, 2004 at 22:11

psdExpress upsd3300

2 REPLIES 2
hpaskal
Associate II
Posted on May 17, 2011 at 11:59

Hi all !

I am developing on the Turbo uPsd DK3300 board with 3334d chip.

I tried to send data through the SPI .

I set pins on Port4 for spi in the PsdExpress program but the data don’t come out from the pins.

Only when I set the registers of Port4 configuration (P4SFS0, P4SFS1) manually in the code , the spi start work through this pins

1) Why do I have to set these regs in my code?

2) Why they don’t have the right value from the merging of the design with the code?

3) Do I have to load some init file after merging the code ?

4) did I missed something here ?

Thanks

joseph2399
Associate II
Posted on May 17, 2011 at 11:59

What you did is correct. This is just the way the part works. First you use PSDsoft to select the function of the port pin from a choice of several options. Then under software control, you choose the function of port 4 as either a port pin or the alternate function. The alternate function can be one of the several options that were available in PSDsoft.