cancel
Showing results for 
Search instead for 
Did you mean: 

MCB 167-NET

vishvas
Associate
Posted on April 06, 2005 at 06:28

MCB 167-NET

2 REPLIES 2
vishvas
Associate
Posted on April 04, 2005 at 14:45

Hi

Can use ST10F168SQ6 in Keil MCB167-net Board.

najoua
Associate II
Posted on April 06, 2005 at 06:28

Hello,

As I know, the Keil MCB167 Evaluation Board introduces you to the Infineon C167CR microcontroller with an on-chip CAN interface.

You can use the ST10F168 MCU but you should pay attention to some differences and hardware requirements.

The C167 CR is nearly similar to the ST10F269 (main difference is pin 84 function and hardware requirement), so you can refer to the attached application note''porting an application from the F168 to the F269'' to discover the differences between the C167CR and the ST10F

Just a question: why you are using the ST10F168 MCU ?( the ST10F269 has more peripherals and functionalities).

CIAO

Najoua

[ This message was edited by: Najoua on 06-04-2005 10:00 ]

________________

Attachments :

Porting_an_application_from_F168_to_F269.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Fs&d=%2Fa%2F0X0000000bYV%2FO5QAOLMxPfMBrsc0I.TwJ6WIeDLbBkaCrVAhVENdKNs&asPdf=false