cancel
Showing results for 
Search instead for 
Did you mean: 

DK3300

maxime239955
Associate
Posted on May 17, 2004 at 22:59

DK3300

2 REPLIES 2
maxime239955
Associate
Posted on May 17, 2011 at 12:00

Hi,

I got DK3300 eval kit for µPSD33xx.

I have some problems to let run the board :

I tested Flashlink with µPSD Softexpress to program Flash on board : all is fine.

I want to test the part in debug mode so I place the jumper in right position. When I try to use Link from Keil, this tool is seen by microvision2 debugger as USB device.

Although, when I try to start debug, an error comes : ''JTAG device chain error''

Is someone can help me ?

joseph2399
Associate II
Posted on May 17, 2011 at 12:00

Please send an e-mail request for an upgrade of the DK3300 kit that includes rev C silicon. The e-mail address is

mailto:apps.psd@st.com

. Please include the following information:

Name

Company Name

Phone Number

Ship to Address

Location (City, State, Country)

uPSD part number of device being used (3334, 3354, etc.)

Application

Projected annual volume (units)

Regards,

uPSD Applications Engineering

[ This message was edited by: uPSD on 18-05-2004 02:32 ]