cancel
Showing results for 
Search instead for 
Did you mean: 

Read memory cycle slow down

dschulmi
Associate II
Posted on February 02, 2006 at 10:42

Read memory cycle slow down

1 REPLY 1
dschulmi
Associate II
Posted on May 17, 2011 at 12:10

In my application the uPSD3234 communicates with a display via the MCU data bus, rd_ and wr_ signals from the uPSD and a CE generated through the internal CPLD. The access times for reading the display are relative slow, the display reacts slower than the external read cycle of the uPSD3234.

The question is, how can I extend the read/write cycles of the uPSD3234 using the same crystal?

Thanks