cancel
Showing results for 
Search instead for 
Did you mean: 

flashlink interface

iyenal
Associate II
Posted on August 09, 2004 at 14:57

flashlink interface

2 REPLIES 2
iyenal
Associate II
Posted on May 17, 2011 at 12:02

Hello,

i was using UPSD3234A on my old project and use flashlink.I use the same programming interface (pullup resistors, serial resistors etc.)as DK3200 board (it has 5V technology) and now i will use UPSD3254BV that works with 3.3V.

Will be there any differences that i must apply with programming interface to use flashlink to program UPSD3254BV.

Regards
joseph2399
Associate II
Posted on May 17, 2011 at 12:02

FlashLink works with both 5.0V and 3.3V devices (it is specified for operation from 2.7 to 5.5V). Pull-up resistors connected to 5V on the 5V version will be connected to 3.3V on the 3.3V version of the device. The hardware interface is the same.