2005-04-19 09:50 PM
2005-04-19 03:04 AM
I'm a bit confused about the maximum allowed clock rates in the STR710, with particular relevance to maximum baud rates on the serial ports.
In the Reference Manual there is a table with PCLK1 set to 20MHz and a maximum baud rate of 625kBaud. Reading the data sheet seems to say that MCLK can go to 50Mhz but PCLK can only go up to 33MHz (is that a recommended value or an absolute maximum value?) Can you tell me what is the maximum recommended clock rate for PCLK1 and 2 and hence for the various peripheral devices? Many Thanks PhilipJ Edited: sorry I've just found the entry in your FAQ about the clock speeds so my question is now a bit simpler, can you set the Baud Rate register UARTn_BR to 1 or is 2 the minimum value allowed (as per the tables in the reference manual)?[ This message was edited by: philipj on 19-04-2005 15:45 ]2005-04-19 03:54 AM
Hello all,
You are right RISC, and the 2 mentioned in the table of the reference manual is just an example 😉 Regards, Hich2005-04-19 05:58 AM
Thanks moderators!!
What happens if you setup the chip for a 32MHz PCLK1 and put 1 in the register? according to the data sheet both conditions are legal and therefore should produce a baud rate of 2Mbits/sec. Does the port somehow choose to work at 625kbaud or just it go into some fault condition? Thanks for your help2005-04-19 09:50 PM
OK,
thanks for the help. It's a bit disappointing because I really wanted 1Mbit/sec for a project that would use a mimimum of 40 ARM7s (maximum of 230!!) talking to each other on an RS485 bus. I will see if my update rates can work at 625kbits/sec. thanks again