cancel
Showing results for 
Search instead for 
Did you mean: 

compiler C to OBJ & HEX (for DK3200)

jendao2000
Associate II
Posted on July 04, 2004 at 10:13

compiler C to OBJ & HEX (for DK3200)

5 REPLIES 5
jendao2000
Associate II
Posted on May 17, 2011 at 12:02

Hello !

i am a newbie in this bussiness and I need your immediate help .

Where can I get a compiler from C to OBJ and HEX?

Thanks for your attention .

jeniok

bbbodekar
Associate II
Posted on May 17, 2011 at 12:02

Hi

I guess you can ask the dealer from where you got the DK3200 to give you an evaluation copy of the C compiler, which would give you both the obj and hex files. You can use Keil C compiler for the same. I dont rember if you get is along with the DK3200 kit. Check it out

Wish you good luck and prosperity in your business!

jendao2000
Associate II
Posted on May 17, 2011 at 12:02

Can you send me the exact link where I can download the compliler?

There are many compilers and I don't find where to download the one I need, I don't know which one I need to compile from C to OBJ and HEX.
sjo
Associate II
Posted on May 17, 2011 at 12:02

There are numerous compilers available for the upsd, any which support 8032 core.

Have a look at www.keil.com, www.raisonance.com, www.tasking.com etc.

If you want to go the free route have a look at sdcc

http://sdcc.sourceforge.net

Regards

sjo
bbbodekar
Associate II
Posted on May 17, 2011 at 12:02

Yes sjo is right.

For DK3200 using UPSD3200, you need to have Keil C compiler. With this, you can compile may devices, e.g Philips 5051 core family , Philips 8032 famliy processors or Cygnal processors etc. So you are not restricted with only 1 type of devices. You get a demo CD from them which has got demo programs and tutorials for using the Keil compiler.

Have fun !