cancel
Showing results for 
Search instead for 
Did you mean: 

STM8 toolchain

fggnrc
Associate II
Posted on April 09, 2008 at 09:38

STM8 toolchain

6 REPLIES 6
alexanderczajor9
Associate II
Posted on May 17, 2011 at 15:01

Hello EtaPhi,

in fact there is a way (not really a hack, but kind of) to use the STVD7 toolset pack 13 for the 1st steps with the STM8A. It is available on the internet in the section www.st.com/mcu under downloads -> ST7 -> software for tools.

Let me know whether you want to use this one or wait for the new toolset pack 14 which is about to be released (should be available within one week).

According to your preference I will give you further instructions.

Best Regards

Alexander

fggnrc
Associate II
Posted on May 17, 2011 at 15:01

The ST site contains only some user manuals and one datasheet.

When the STM8 toolchain will be avalilable?

fggnrc
Associate II
Posted on May 17, 2011 at 15:01

Hello Alexander.

I prefer to wait the new STVD7 and do a clean install.

I thank you for the quick answer.

EtaPhi

luca239955_st
Associate III
Posted on May 17, 2011 at 15:01

C compiler is

http://www.cosmicsoftware.com/download_stm8_16k.php

(free up to 16k).

Regards,

Luca (Cosmic)

Viktor POHORELY
ST Employee
Posted on May 17, 2011 at 15:01

Toolchain is already available on ST website. It is called now STVD, instead of STVD7, in order to indicate support for more families.

Enjoy

http://www.st.com/mcu/familiesdocs-15.html#Software for Toolsmdt

Viktor POHORELY
ST Employee
Posted on May 17, 2011 at 15:01

RLINK is supported as an interface, but there is a need for adaptor. Therefore, RLINK 3.4 is recommended for professional use.

Anyway, there is a description of the adaptor connection available on Raissonance website

http://www.raisonance.com/Forum/punbb/viewtopic.php?id=2449

But not all information were clearly stated (as today), so there is additional info:

- a pull up resistor is mandatory to support data signal

- Pins 6,12 and 15 should be connected together

- there should be no difference in supply voltage between application and Rlink

- overload resistors should protect the signals (between 0,5 to 1k)