cancel
Showing results for 
Search instead for 
Did you mean: 

Format of AXF-Files

marcus23
Associate II
Posted on October 05, 2004 at 05:42

Format of AXF-Files

2 REPLIES 2
marcus23
Associate II
Posted on September 30, 2004 at 11:04

Hello everybody,

I got a problem with the AXF files produced by the eval-license of the ST-Preview edition of RVDS. After our eval-license expired we bought the full version of RVDS2.1 from ARM. Now I can´t load the axf-files produced by the older ST-version into the STR710. I get the following error:

C:\ARM\STR71x\Projects\I2C-Demo\Debug\I2C-Demo.axf is not correct object type.

I even can´t load the demo-application from the ST-website anymore.

So, does anyone know if there are any differences between the axf-files of RVDS2.0 an RVDS2.1?The header of the old and the new axf-files seems to be different. Or is it something ST-specific?

Here the first bytes of a RVDS2.0-file:

F7 4F 52 43 01 01 01

and here the first bytes of a RVDS2.1 file:

7F 45 4C 46 01 01 01

Just changing the bytes that differ in the header doesn´t work. Maybe someone could help me.

Thanks
marcus23
Associate II
Posted on October 05, 2004 at 05:42

Hello ibtiss,

now as you mentioned I see the difference between ''RVDS'' and ''RVDK''. So I have to say, that I were using the 45-days preview edition of the RealView Developer KIT, and now I have the RealView Developer SUITE. Is there no possibility to convert the RVDK-image to a RVDS-image?

Thanks for your help,

Marcus