cancel
Showing results for 
Search instead for 
Did you mean: 

Need some help in flashing str71xdemo_gp.axf

spectrum_hp2004
Associate II
Posted on August 05, 2004 at 09:00

Need some help in flashing str71xdemo_gp.axf

3 REPLIES 3
spectrum_hp2004
Associate II
Posted on August 05, 2004 at 05:21

Hi

I am trying to flash the code (str71xdemo_gp.axf) to ST Micro's evaluation board MB393B through ARM realView ICE ( JTAG Emulator).

Processor: STR710FZ2T6.

I want to use the embeded (internal) flash.

During the time of flashing I have maintained the following boot settings: ( RAM MApped at 0h)

BOOTEN:1

BOOT0:0

BOOT1:1

I could succesfully flash the code.

Swicthing off the supply, I changed my boot configuration settings to

USER mode ( Flash mapped at 0h) to run the program.

BOOTEN:0

BOOT0:0

BOOT1:0

But I am not finding anything on the LCD Display.

I am not in a position to findout whether the program is correctly booting from internal flash.

Can anybody help me in giving the correct procedure( step-by-step) of

flashing this code, all the necessry H/W settings to be maintained on the board.

Also tell me Is this, the only file ( str71xdemo_gp.axf)I have to use for flashing or any other associated files are required along with this. If so please mention the same.
spectrum_hp2004
Associate II
Posted on August 05, 2004 at 06:34

Hi

I have used this evaluation board for other purposes during my project development.The board is working fine.

But during that time i was using the debugging environment.

Now I am trying to flash the code. The board is not displaying anything.

Let me try LCD.zip code.

But Is it enough if I just flash the code present inside this zip folder (lcd.zip)? Or any other files required?

What should be the boot configuration settings?
spectrum_hp2004
Associate II
Posted on August 05, 2004 at 09:00

As you sugeested we used this file in debugging mode.

We were able to see some segments of the LCD blinking

We could monitor Enable signal toggling at the LCD ( 6'th Pin).

( I think some portion of LCD has gone bad).

Now in the second phase I flashed the same code.

My expectation is to observe the same phenomenon on the LCD display.

But I didnt see any blinking on the LCD screen which I observed in the previous experiment.

Could you help me in this regard...