cancel
Showing results for 
Search instead for 
Did you mean: 

iFLASH Timing Question

urik
Associate II
Posted on March 06, 2006 at 10:20

iFLASH Timing Question

3 REPLIES 3
urik
Associate II
Posted on March 06, 2006 at 10:11

Hello,

i found in the data sheet that if i use the 64MHz frequency i need to add 1 wait state to the xFLASH, 2 wait states for the XRAM1/2, but what about the iFLASH and iRAM i could not find any data to them, can i assume that they work with 0 wait states?

thanks,

Uri.

najoua
Associate II
Posted on March 06, 2006 at 10:18

Hello,

IFLASH and IRAM (Non XBUS peripherals in general) don't need Waitstates.

The IFlash module offers a fast access time, allowing zero wait-state access with CPU frequency up to 64 MHz.

XFLASH and XRAM need waitstates because they are seen as external peripherals even they are internal.

Regards,

Najoua.

[ This message was edited by: Najoua on 06-03-2006 14:52 ]

urik
Associate II
Posted on March 06, 2006 at 10:20

Thank you very much for the prompt answer.

regards,

Uri.