cancel
Showing results for 
Search instead for 
Did you mean: 

Linking error in Hiware compiler

raunaque
Associate II
Posted on January 01, 2005 at 06:51

Linking error in Hiware compiler

1 REPLY 1
raunaque
Associate II
Posted on January 01, 2005 at 06:51

Hi all

i am trying to compile a piece of code on the Hiware compiler. i am trying to call a function but i get the error ''ERROR L2009: Out of allocation space in segment BUFFER1_EP2_512 at address 1A50'' . i am also pasting the *.MAP file which is generated by the compiler. it is below this message .Can anybody interpret it and what misatke i am committing or i am using more RAM than allocated .

Any help

ALLOCATION FOR PROGRAM USB_FS_7265_32K.abs ABORTED BECAUSE OF SECTION EXHAUSTION

******************************************************

SEGMENT USE IN OBJECT-ALLOCATION SECTION

------------------------------------------------------

SEGMENT ''EP2_BUF''

Data_EP2 200 78 ( 0) EP2_BUF

SEGMENT ''BUFFER0_EP2_512''

Buffer_0 1650 200 ( 0) BUFFER0_EP2_512

SEGMENT ''BUFFER1_EP2_512''

Buffer_1 1850 200 ( 0) BUFFER1_EP2_512