cancel
Showing results for 
Search instead for 
Did you mean: 

Can you run code from Serial Flash with STR71x

mike6
Associate II
Posted on May 10, 2005 at 05:44

Can you run code from Serial Flash with STR71x

1 REPLY 1
mike6
Associate II
Posted on May 06, 2005 at 19:05

We are going to use the STR71x and I would like to use the M25P

serial flash, but I do not see a way to use a serial flash for code storage and execute from the flash. Is there a way to execute code and boot from serial flash via the SPI bus? Booting from onboard flash would be fine too, but can I run code from the serial SPI flash without transferring the code to RAM or somewhere else to run it?