cancel
Showing results for 
Search instead for 
Did you mean: 

RVDS 2.2 /Multi ICE with STR912FW44

cgrun
Associate II
Posted on October 30, 2006 at 11:23

RVDS 2.2 /Multi ICE with STR912FW44

2 REPLIES 2
cgrun
Associate II
Posted on May 17, 2011 at 09:33

Hello,

1/ Can somebody could provide me the necessary files to support an STR912 using a Full version of RVDS ?

I think I just need .FME (Flash methods) and .BCD (board/chip definition).

2/ I see that tere is some specific register that permit to choose the order for the flashs. CAPS permit to porgram these. But are there any manner to access this using an arm program / or using RVDS ?

Do I need buy a flashlink or rlink to manage this ?

Sincerely

Chris.

bayram
Associate II
Posted on May 17, 2011 at 09:33

Hi,

The number of documentations for STR9 is less than those for STR7. For STR7, we are able to find the files you need under ''Documents and files for family STR7/Software Patches/RVDK 2.1 (STR73xF)''. However, there is no file for the STR9 about this; it must be so moderators can help.

Best Regards