cancel
Showing results for 
Search instead for 
Did you mean: 

Changing Baud rate

qbarry
Associate II
Posted on April 28, 2008 at 14:31

Changing Baud rate

1 REPLY 1
qbarry
Associate II
Posted on May 17, 2011 at 09:52

Help!

I am trying to configure the serial port 0 to function at different baud rates. The port is functioning, however when I change the baud rate it only prints 0. The first stream at 9600 is correct. I then step up the baud rate to 19200, 38400, etc. Only 9600 works. If I init the port to 19200 then only 19200 works.

This seems a bit buggy to me. Anyone had the same issues - or can anyone help me out here?

Regards

Quentin