cancel
Showing results for 
Search instead for 
Did you mean: 

RLINK - FLINK

paolo_capobianco
Associate II
Posted on April 06, 2006 at 19:04

RLINK - FLINK

2 REPLIES 2
paolo_capobianco
Associate II
Posted on May 17, 2011 at 12:07

Ciao,

I have problems in using the RLINK to program a uPSD3233B on board.

I'm able to erase , execute a blank test, and on a programmed part execute the verify, but when I try to program it I always get the following error:

PSDsoft Express 8.30 Copyright (C) 1993-2004 STMicroelectronics, Inc. All Rights Reserved.

DATE : 06/15/2005 TIME : 12:22:24

Device 1 : ( 4 pins )

Program ...

Erasing ...

Programming/Verifying...

fail

Program/verify operation unsuccessful ...

ERROR: Data (0600)

Hint: Programming failure.

Time elapsed : 6 sec.

By the way, if I use the Flashlink on the same board, I've no problems.

I also changed the Rlink, assuming it was damaged, but no changes.

Any idea?

Thanks

rtarrant
Associate II
Posted on May 17, 2011 at 12:07

I am getting this same problem. I can't explain why. The osf file is created correctly. I am using a PSD4256G6V.