cancel
Showing results for 
Search instead for 
Did you mean: 

ST7LITE15BF0, option bytes and InDART-STX ?

jps
Associate II
Posted on October 17, 2007 at 14:14

ST7LITE15BF0, option bytes and InDART-STX ?

1 REPLY 1
jps
Associate II
Posted on October 17, 2007 at 14:14

Hi,

I have developped a first application with the ST7LITE15BF0 and it works fine!

Just a last problem : When I connect my target board to my InDART-STX debugger, if I use the option bytes it doesn't works (dial stopped between InDART and my board). If I don't use option bytes and use the InDART clock applyed on pin 20 of the controller, it works. So I can debbug an then I program the FLASH and the option bytes, I deconnect the InDART and it works?

With old cards with ST7LITE05, I can debbug with the option bytes programmed using the internal RC as oscillator when the InDART is connected? What are the diferences and why this behaviour differences between the 2 micro's? Is there any possibility to debbug a ST7LITE15BF0 with InDART using the micro internal RC?

Thank you to give me an answer.

Regards

Whitebull